Removing the Drawout Device
Device Removal
| NOTICE |
|---|
|
HAZARD OF EQUIPMENT DAMAGE
The chassis must be securely fastened when installing
or removing the device.
Failure to follow these instructions can result in equipment damage.
|
|
Step |
Action |
|
|---|---|---|
|
1 |
With the device in the disconnected position, discharge the closing spring by pressing the closing pushbutton. If the closing spring is charged, the device closes. |
![]() |
|
2 |
Press the opening pushbutton to open the device. |
![]() |
|
3 |
Pull out the rails to the maximum by pulling on the drawout grips. The moving part of the drawout device stays in disconnected position in the chassis. |
![]() |
|
4 |
Pull out the moving part of the drawout device to the maximum, by rolling it along the rails. Result: The device is supported on the rails, clear of the chassis and ready to be lifted. |
![]() |
Lifting the Device
Both the device and chassis have a carrying grip for lifting. To lift the device, use an overhead lifting device attached to the carrying grip, following the directions given in this section.
DANGER |
|---|
|
HAZARD OF DEVICE FALLING
Failure to follow these instructions will result in death or serious injury.
|
Lift the device from the chassis rails by using the carrying grip located on the sides of the device.

Device Weights
The following table shows the weights of the different devices available.
|
Number of poles |
Device |
MTZ1 |
|---|---|---|
|
3P |
Moving part (Drawout) |
14 kg |
|
Chassis |
16 kg |
|
|
Fixed Device |
14 kg |
|
|
4P |
Moving part (Drawout) |
18 kg |
|
Chassis |
21 kg |
|
|
Fixed Device |
18 kg |




DANGER