Drawout MasterPacT MTZ1 Device Status
Drawout Device Handling Conditions
Connection or disconnection of the drawout device requires insertion of the racking handle. When interlocks, padlocks, or an open door lock are in place, the racking handle cannot be inserted.
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Drawout Device Positions
The indicator located on the front of the chassis locally signals the position of the device in the chassis.
Drawout Device Position Contacts
The position of the device in the chassis is indicated remotely by the following position contacts:
-
CE: connected position
-
CT: test position
-
CD: disconnected position
The state of the position contacts changes according to the device position during racking-in and racking-out operations, as shown in the diagram below.
A Device in connected position
B Separation of the main circuits
C Device in test position
D Separation of auxiliary circuits
E Device in disconnected position
Drawout Device Position Contacts Without EIFE Ethernet Interface
Without EIFE Ethernet interface, optional position contacts can be added as follows:
-
2 CD disconnected position contacts
-
3 CE connected position contacts
-
1 CT test position contact
Drawout Device Position Contacts With EIFE Ethernet Interface
With EIFE Ethernet interface, 2 optional CE connected position contacts can be added.
Chassis Management Function
The chassis management function is used to:
-
Record and check the position of the moving part of the drawout device in the chassis
-
Provide information about preventive maintenance actions
-
Notify the remote controller about the position of the drawout device
The chassis management function is performed by:
-
The EIFE Ethernet interface, refer to DOCA0106•• Enerlin'X EIFE - Embedded Ethernet Interface for One MasterPacT MTZ Drawout Circuit Breaker - User Guide.
-
The IO module, refer to DOCA0055•• Enerlin'X IO - Input/Output Application Module for One Circuit Breaker - User Guide.
DANGER