Fixed Device
Fixed Device Description
The following image shows the standard version of the fixed device (no optional accessories).
Fixed Device Accessories Description
The following image shows the accessories available for the fixed device.
The following images zoom in on the accessories for the fixed device:
Fixed Device Terminal Block Description
Assignment of Terminal Blocks
The following table describes the assignment and the availability of the terminal blocks for fixed circuit breakers and switch-disconnectors:
-
Standard terminal blocks and the associated accessories are delivered with the device.
-
Optional terminal blocks are delivered with the device only if the associated optional accessories are installed in the device.
-
N/A indicates that the terminal blocks and the associated optional accessories are not compatible with the device.
|
Marking |
Description |
Circuit breaker |
Switch-disconnector |
|---|---|---|---|
|
COM |
Terminal block for the external power supply of the MicroLogic X control unit |
Standard |
N/A |
|
or ULP port module |
Optional |
N/A |
|
|
UC1 |
Zone selective interlocking (ZSI), rectangular sensor for earth-leakage protection, or MDGF module input |
Standard |
N/A |
|
UC2 |
Neutral external sensor, rectangular sensor for earth-leakage protection, or MDGF module input |
Standard |
N/A |
|
SDE2/RES |
SDE2 additional fault-trip indication contact or RES electrical remote reset |
Optional |
N/A |
|
M2C/ESM/UC4 |
M2C programmable contacts, ESM ERMS switch module, or external voltage connector |
Optional |
N/A |
|
UC3 |
External voltage connector |
|
N/A |
|
SDE1 |
SDE1 fault-trip indication contact |
Standard |
N/A |
|
MN/MX2 |
MN undervoltage release or MX2 opening voltage release |
Optional |
Optional |
|
MX1 |
MX1 opening voltage release |
Optional |
Optional |
|
XF |
XF closing voltage release |
Optional |
Optional |
|
PF |
PF ready-to-close contact |
Optional |
Optional |
|
MCH |
MCH gear motor |
Optional |
Optional |
|
OF1-OF4 |
4 OF indication contacts |
Standard |
Standard |