Locking the Device in Open Position with Keylocks
Description
Optional keylocks can be used:
-
To lock one MasterPacT MTZ1 in the open position. When locked the device cannot be closed either locally with the closing pushbutton or remotely.
-
To interlock several MasterPacT MTZ1 devices locked with the same key.
To use keylocks to lock the device in the open position, an optional OFF-position locking accessory is necessary.
This accessory is not compatible with the VCPO OFF-position padlocking accessory, the two accessories cannot be used at the same time.
This accessory is not compatible with the BPFE closing pushbutton.
VSPO OFF-Position Locking Accessory
The OFF-position locking accessory is an optional accessory
that is mounted on the front of the device.
The OFF-position keylocking accessory can be fitted with either:
-
One keylock.
-
Two keylocks with identical keys or different keys.
The following types of keylocks can be fitted:
|
Ronis keylock ![]() |
Profalux keylock ![]() |
Castell keylock (keylock not provided) ![]() |
Kirk keylock (keylock not provided) ![]() |
For information on the accessory installation, consult the instruction sheet on the Schneider Electric website: NVE56770.
Locking the Device in the Open Position
For devices equipped with two keylocks, locking with one key is sufficient to lock the device in the open position.