DOCA0100EN-08

Mismatch Protection

Description

Mismatch protection allows the installation of a MasterPacT MTZ1 device only in a chassis with compatible characteristics.

Mismatch protection offers 35 different combinations that can be selected so that a device can only be mounted on a chassis with the matching combination.

Accessory

The use of mismatch protection is optional. One mismatch protection accessory is required for each device.

For information on the accessory installation, consult the instruction sheet available at Schneider Electric website: NVE35465.

Pin Location of Mismatch Protection

The following illustration shows the pin location on the chassis and device, respectively.

The pin combination selected on the chassis must correspond to the pin combination selected on the device (see following table). For example, the combination 12 on the chassis corresponds to the combination CDE on the device.

Pins on the chassis are labeled 1, 2, 3, 4, 5.

Pins on the device are labeled A, B, C, D, E.

TechPub writer: update graphic above once updated IS is available.

Recommended Pin Combinations

The following are the recommended pin combinations:

Pins on chassis

Pins on device

Pins on chassis

Pins on device

45

ABC

15

BCD

35

ABD

14

BCE

34

ABE

145

BC

345

AB

13

BDE

25

ACD

135

BD

24

ACE

134

BE

245

AC

12

CDE

23

ADE

125

CD

235

AD

124

CE

234

AE

123

DE

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.