Installation
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Site Selection and Preparation
Site preparation is essential for proper installation and operation of the equipment. To prepare the site for installation, be sure to:
-
Compare the site plans and specifications with the motor controller drawings to be sure there are no discrepancies.
-
Check the site to verify that the equipment will fit properly and withstand the weight of the equipment.
-
Ensure that the floor is level within 1/16 in. per ft. (2 mm per 305 mm), or a maximum of 1/4 in. (6 mm) within the area of the controller lineup. If the floor is not within the tolerances, use shims or other means to ensure equipment is installed on level.
-
Ensure that the installation site meets all environmental specifications for the enclosure’s NEMA type rating, and all other applicable NEMA/CEMA rating.
-
Ensure the site is in compliance with seismic hazard for site specific locations as defined by the current edition of the International Building Code or NFPA 5000 or relevant local building code or consulting engineer of record.
-
Allow working space clearance per National Electrical Code (NEC) or local standard. Minimum clearances must meet all local and national requirements.
-
This equipment is front accessible only and does not have rear access.
-
Provide area ventilation, heating, and air conditioning to maintain the ambient temperature around the equipment between 0°C (32°F) and 40°C (104°F).
-
Adequate lighting and convenience outlets with the correct power source should be available near the equipment.
-
Ensure that the power cables have the correct NEC/CSA current rating for the unit being installed. Depending on the model, the power cables can range from a single #14 AWG conductor to four 750 MCM cables. Consult local and national codes for selecting wire size.
-
Route sewer, water, and steam lines away from the equipment.
-
Provide floor drains to help prevent water buildup.
Equipment Installation for Seismic Applications
Introduction
Seismic certification is an optional feature in the MotorSet product line that provides seismic conformance options to any of the North American and International building codes and seismic design standards identified in List of Supported Regional Building Codes and Seismic Design Standards. A MotorSeT product that is seismic certified has been certified to the seismic requirements of the listed code per the manufacturer’s certificate of compliance (CoC). Equipment compliance labels and CoC’s are provided with all seismic certified MotorSeT products. Refer to the equipment CoC for certification details and applicable seismic parameters. To maintain the validity of this certification, the installation instructions provided in this section must be followed.
List of Supported Regional Building Codes and Seismic Design Standards
|
Country/Region |
Code Reference ID |
Code Name |
|---|---|---|
|
Argentina |
INPRES-CIRSOC103 |
Argentinean Standards for Earthquake Resistant Constructions |
|
Australia |
AS 1170.4–2007 (R2018) |
Structural design actions, Part 4: Earthquake actions in Australia |
|
Canada |
NBCC |
National Building Code of Canada |
|
Chile |
NCh 433.Of1996 |
Earthquake resistant design of buildings |
|
China |
GB 50011-2010 (2016) |
Code of Seismic Design of Buildings |
|
Colombia |
NSR-10 Titulo A |
Colombian Regulation of Earthquake Resistant Construction |
|
Europe |
Eurocode 8 EN1998-1 |
Design of structures for earthquake resistance — Part 1: General rules, seismic actions and rules for buildings |
|
India |
IS 1893 (Part 1): 2016 |
Criteria for Earthquake Resistant Design of Structures Part 1 General Provisions and Buildings |
|
Indonesia |
SNI 1726:2019 |
Earthquake Resistance Planning Procedures for Building and Non-building Structures |
|
Japan |
Building Standard Law |
The Building Standard Law of Japan |
|
Mexico |
CFE MDOC-15 |
Civil Works Design Manual, Earthquake Design |
|
New Zealand |
NZS 1170.5:2004+A1 |
Structural design actions, Part 5: Earthquake actions — New Zealand |
|
Peru |
N.T.E. - E.030 |
National Building Code, Earthquake-Resistant Design |
|
Russia |
CП 14.13330.2018 |
Building norms and regulations: Construction in seismic regions |
|
Saudi Arabia |
SBC 301 |
Saudi Building Code, Loads & Forces Requirements |
|
Taiwan |
CPA 2011 |
Seismic Design Code and Commentary for Buildings |
|
Turkey |
TBEC-2018 |
Turkey Buildings Earthquake Standard |
|
United States |
IBC per ASCE 7 |
International Building Code—IBC |
|
CBC per ASCE 7 |
California Building Code—CBC |
|
|
UFC per DoD |
Uniform Facilities Criteria—UFC |
Responsibility for Mitigation of Seismic Damage
The MotorSeT equipment is considered a nonstructural building component as defined by regional building codes and seismic design standards. Equipment capacity was determined from tri-axial seismic shake-table test results in accordance with the International Code Counsel Evaluation Service (ICC ES) Acceptance Criteria for Seismic Certification by Shake-Table Testing of Non-structural Components (ICC-ES AC156).
An equipment importance factor, Ip, that is greater than one (Ip > 1.0) is assumed and indicates that equipment functionality is required after a seismic event and after seismic simulation testing. This importance factor is applicable for designated seismic systems (for example, special certification) servicing critical infrastructure and essential buildings where post-earthquake equipment functionality is a requirement.
Incoming and outgoing bus, cable, and conduit must also be considered as related but independent systems. These distribution systems must be designed and restrained to withstand the forces generated by the seismic event without increasing the load transferred to the equipment. For applications where seismic hazard exists, it is preferred that bus, cable, and conduit enter and exit the bottom of the equipment enclosure.
Seismic certification of nonstructural components and equipment by Schneider Electric is just one link in the total chain of responsibility required to maximize the probability that the equipment will be intact and functional after a seismic event. During a seismic event the equipment must be able to transfer the inertial loads that are created and reacted through the equipment’s force resisting system and anchorage to the load-bearing path of the building structural system or foundation.
Anchorage of equipment (for example, nonstructural supports and attachments) to the primary building structure or foundation is required to validate seismic conformance. The construction site structural engineer or engineer of record (EOR) or the registered design professional (RDP) is responsible for detailing the equipment anchorage requirements for the given installation. The installer and manufacturers of the anchorage system are responsible for assuring that the mounting requirements are met. Schneider Electric is not responsible for the specification and performance of equipment anchorage systems.
Tie-Down Points for Rigid Floor Mounted Equipment
The equipment enclosure provides anchorage tie-down points to accept anchor attachments to the building structure or foundation. Indoor and outdoor enclosures provide enclosure base frame clearance holes for bolted anchorage attachments as shown in job drawings.
Equipment installations of single, stand-alone sections must be anchored using all enclosure tie-down points as shown in job drawings for indoor and outdoor applications respectively. Equipment installations of multiple-section lineups (2 or more MotorSeT units bolted together) may not require every tie-down point to be used and specifics will be shown in the job drawings.
Equipment installations using welded supports and attachments in lieu of bolted supports and attachments must ensure the weld locations are distributed similarly to the locations of enclosure anchorage clearance holes. Welded supports and attachments must be properly sized to ensure the weldment withstand capacity exceeds the earthquake demand at the location of equipment installation. Precautions shall be made to properly vent and shield the equipment enclosure during the field welding process. Schneider Electric is not responsible for equipment damage caused by field welded supports and attachments.
Anchorage Assembly Instructions
The bolted anchor assembly view depicted in job drawings illustrates the equipment’s as-tested attachment to the seismic shake-table test fixture. The equipment seismic rated capacity, as stated on the Schneider Electric CoC, was achieved with the identified size and grade attachment hardware. For bolted attachments, the use of grade 5 or better hardware with thick, hardened, Belleville conical spring washers, where specified in job drawings, are required to maintain seismic conformance. Field installed equipment attachment and support detailing shall be in accordance with the anchorage system requirements as defined by the construction site EOR or RDP.
Before You Start
Read and understand the following information before performing motor starter installation procedures.
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
Before installing the ATL motor starter, do the following:
| NOTICE |
|---|
|
starter or motor Damage
Failure to follow these instructions can result in equipment damage.
|
EMC Compliance
To comply with the European Electromagnetic Compatibility (EMC) standards, follow these guidelines.
Guidelines for EMC Installation Compliance
|
Function/Feature |
Guideline |
|---|---|
|
Enclosure |
Install the product in a grounded metal enclosure. |
|
Grounding |
Connect a grounding conductor to the screw or terminal provided as standard on each controller. See power wiring schematic for grounding provision location. |
|
Wiring |
See Wiring Practices. |
|
Filtering |
To comply with Conducted Emission Limits (CE requirement), a high voltage (rated controlled voltage or greater) 0.1 uF capacitor must be connected from each input line to ground it at the point where the line enters the cabinet. |
Applicable Standards and Codes
|
Electromagnetic Compatibility (EMC) |
|
Wiring
Wiring Practices
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
When wiring the motor controller, follow these guidelines:
-
Never connect input AC power to motor controller (load) output terminals T1/U, T2/V, or T3/W.
-
Power wiring to the load should be separated from all other wiring inside the enclosure.
-
Do not run power wiring and control wiring (or any wiring group) in the same conduit. The minimum spacing between metallic conduits containing different wiring groups should be 3 in. (8 cm).
-
The minimum spacing between different wiring groups in the same tray should be 6 in. (15 cm).
-
When running wiring outside an enclosure, the wiring should be run in metallic conduit or have shielding/armour with equivalent attenuation (density).
-
If the control wiring must cross the motor controller or mains cables, the wiring should cross at an angle of 90°.
Power Cables
Power wiring refers to wires/cables connected to the line and load terminals that normally carry 2200–7200 Vac. When selecting power wiring:
-
Use only cables that meets UL or CSA requirements
-
Grounding must be in accordance with NEC, CEC or local codes. If multiple devices are installed near each other, each must be grounded. Make sure not to form a ground loop. The grounds should be connected in a star configuration.
Control Wiring
Control wiring refers to wires connected to the control terminal strip that normally carry 24–115 V.
Signal Wiring
Signal wiring refers to wires connected to the control terminal strip with low voltage signals (below 15 V).
-
Wires should be shielded/armour to help prevent electrical noise interference, which can cause improper operation or nuisance tripping.
-
Signal wiring inside the enclosure should routed to maintain maximum separation as feasibly possibly from control and power wiring.
-
Use signal wiring with the highest possible voltage rating (at least 300 V rating).
Joining Shipping Splits
After properly preparing the site, field assemble the shipping splits.
-
Shipping splits are made to provide convenience for the installer.
-
The installer must properly align, level, and bolt the units together and to the concrete floor.
-
The installer must properly install the interconnection bus and any interconnection secondary control, instrumentation, heaters, wiring, etc. Schneider Electric provides all materials for interconnections including hardware, bus, insulation and internal secondary wiring.
-
Install all interconnections in accordance with drawings and wiring diagrams provided with the equipment.
Accessing the Isolation Section Compartment—Standard and Compact Configurations
To access the isolation section compartment, follow these steps:
-
If an optional keylock is provided, use the key to unlock the isolation section cover.
-
Remove the disconnector switch operator handled from the cover.
-
Remove the four bolts attaching the isolation section cover to the unit and set aside.
-
Remove the cover and set it aside.
-
When reversing the above steps to install the medium voltage isolation section cover, make sure to fully tighten the bolts on the cover, tighten the hardware attaching the operator handle, and lock the cover lock if a keylock option is included.
Accessing the MV Compartment—Standard and Compact Configurations
To access the medium voltage compartment, follow these steps:
-
If an optional keylock is provided, use the key to unlock the medium voltage door.
-
Using a screwdriver or nut driver, loosen the screws on the door closure brackets and slide the door closure brackets off the door flange tabs.
-
The medium voltage door can now be opened.
-
When reversing the above steps to close the medium voltage door, make sure to slide brackets over the door flange tabs before fully tightening the door closure bracket screws and lock the door lock, if a keylock option is included.
Accessing the MV Compartment—Dual Configuration
To access the medium voltage compartment, follow these steps:
-
If an optional keylock is provided, use the key to unlock the medium voltage door.
-
Remove the screws in the upper and lower right corner of the medium voltage door.
-
Lift and rotate the lift and turn latch up and pull the door open.
-
When reversing the above steps to close the medium voltage door, make sure to fully tightening the screws in the upper and lower right corner of the door and lock the door lock (if a keylock option is included).
Accessing the Low Voltage Compartment—Standard and Compact Configurations
To access the low voltage compartment, follow these steps:
-
If an optional keylock is provided, use the key to unlock the low voltage door.
-
Using a screwdriver or nut driver, loosen the screws on the door closure brackets and slide the door closure brackets off the door flange tabs.
-
The low voltage door can now be opened.
-
When reversing the above steps to close the low voltage door, make sure to slide brackets over the door flange tabs before fully tightening the door closure bracket screws and lock the door lock, if a keylock option is included.
Accessing the Low Voltage Compartment—Dual Configuration
To access the low voltage compartment follow these steps:
-
If an optional keylock is provided, use the key to unlock the low voltage door.
-
Rotate the door locking knobs 90 degrees.
-
The low voltage door can now be opened.
-
When reversing the above steps to close the low voltage door, make sure to rotate the door locking knobs back to their original positions and lock the door lock, if a keylock option is included.
Anchoring the Equipment
Anchoring and Joining the Shipping Splits
Follow the steps below for instructions on anchoring the units.
-
Review the assembly drawings to ensure that the equipment shipping splits will be assembled in the correct order.
NOTE: If the equipment will be connected to an existing lineup, mount the connecting section or shipping split first. -
Locate and anchor the first shipping split.
For seismic hazard designated locations, each section must be anchored per details supplied by the Engineer of Record to the load-bearing path of the building structure system. Use grade 5 or better hardware with thick, hardened, Belleville washers as specified in the job drawings to maintain equipment seismic ratings.
For non-seismic hazard locations, 1/2 in. (12 mm) grade 5 or higher bolts are recommended; however, 3/8 in. (10 mm) grade 5 bolts are permissible.
NOTE: Be sure to mount all shipping splits on the same plane and level them to verify that they are properly connected. -
Locate the next shipping split according to the assembly job drawings.
-
Level the shipping split and join it to the previously installed shipping split. Apply vertical and horizontal gasket and bolt enclosures together using 3/8 in. or M10 mm hardware in all eight locations (see Gasket and Joining Enclosure Mounting Hole Locations).
Bus Connections
When shipping several sections of switchgear for a lineup, it is necessary to disconnect the main bus before shipping.
-
It is important that the MotorSeT equipment be anchored in place before reconnecting the main bus.
-
It is essential that the bus bar connections be securely bolted to create the necessary pressure for proper conductivity between the bus bars.
Refer to the provided drawings and Bolt Torque Values for Bus Connections for more information.
Follow these steps for all field-assembled joints in primary conductors, regardless of material or insulation method:
-
Wipe the bus surface clean with a lint-free cloth. Do not use sandpaper or any abrasive on the plated surface. Avoid touching the cleaned surface as much as possible.
-
Join the clean contact surfaces by using the hardware provided, see Busbar Connections for more information.
-
Use the torque values as listed in Bolt Torque Values for Bus Connections.
NOTE: The torque values in Bolt Torque Values for Bus Connections do not apply to the contact mechanism of the disconnector switch.
Legend — Busbar Connections Diagram
|
Call-out |
Description |
|---|---|
|
A |
Lock washer* |
|
B |
Flat washer* |
|
C |
Busbars |
|
D |
Bolt |
|
E |
Nut |
Bolt Torque Values for Bus Connections
|
Bolt Material |
Torque in Feet (ft.) — Pounds (lbs.) for bolt size |
||||
|---|---|---|---|---|---|
|
1/ 4-20 |
5/16-18 |
3/8-16 |
1/ 2-13 |
5/8-11 |
|
|
Steel |
5 |
12 |
20 |
50 |
95 |
|
Silicon bronze |
5 |
10 |
15 |
40 |
55 |
Power Wiring Connections
Power wire (cable) should be selected based on the FLA of the load. Wire derating may be necessary based on ambient temperatures.
For assistance in selecting the correct wire size, consult local and national codes.
DANGER |
|---|
|
HAZARD OF ELECTRICAL SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
To connect the line side and load side power cables, follow these steps:
-
Route the power cables through a connector into the enclosure.
-
Strip the cable insulation from the end of cable per the lug manufacturer's instructions.
-
If recommended by the lug manufacturer, apply anti oxidation paste to the cable prior to crimping lug to cable.
-
Connect the motor load cables to the T1, T2 and T3 lugs or terminals.
-
Connect the power source cables to the L1, L2 and L3 lugs or terminals.
Compression Lugs
The following is a list of recommended crimp-on wire connectors for copper wire manufactured by Penn-Union Corp.:
Single Hole Compression Lugs
|
Wire size |
Part number |
|---|---|
|
1/0 |
BLU-1/0S20 |
|
2/0 |
BLU-2/0S4 |
|
3/0 |
BLU-3/0S1 |
|
4/0 |
BLU-4/0S1 |
|
250 MCM |
BLU-025S |
|
300 MCM |
BLU-030S |
|
350 MCM |
BLU-035S |
|
400 MCM |
BLU-040S4 |
|
450 MCM |
BLU-045S1 |
|
500 MCM |
BLU-050S2 |
|
600 MCM |
BLU-060S1 |
|
650 MCM |
BLU-065S5 |
|
750 MCM |
BLU-075S |
|
800 MCM |
BLU-080S |
|
1000 MCM |
BLU-100S |
|
1500 MCM |
BLU-150S |
|
2000 MCM |
BLU-200S |
Torque Values for Power Wiring Terminations
Slotted Screws and Hex Bolts — Tightening Torque Values
|
Wire size installed in conductor |
Tightening torque, in.-lb (N•m) |
||||||||
|---|---|---|---|---|---|---|---|---|---|
|
Slotted head No. 10 and larger |
Hexagonal head-external drive socket wrench |
||||||||
|
AWG or kcmil |
(mm2) |
Slot width ≤ 0.047 in. (1.2 mm) and slot length ≤ 0.25 in. (6.4 mm) |
Slot width > 0.047 in. (1.2 mm) or slot length > 0.25 in. (6.4 mm) |
Split-bolt connectors |
Other connectors |
||||
|
18–10 |
(0.82–5.3) |
20 |
(2.3) |
35 |
(4.0) |
80 |
(9.0) |
75 |
(8.5) |
|
8 |
(8.4) |
25 |
(2.8) |
40 |
(4.5) |
80 |
(9.0) |
75 |
(8.5) |
|
6–4 |
(13.3–21.2) |
35 |
(4.0) |
45 |
(5.1) |
165 |
(18.6) |
110 |
(12.4) |
|
3 |
(26.7) |
35 |
(4.0) |
50 |
(5.6) |
275 |
(31.1) |
150 |
(16.9) |
|
2 |
(33.6) |
40 |
(4.5) |
50 |
(5.6) |
275 |
(31.1) |
150 |
(16.9) |
|
1 |
(42.4) |
– |
– |
50 |
(5.6) |
275 |
(31.1) |
150 |
(16.9) |
|
1/0–2/0 |
(53.5–64.4) |
– |
– |
50 |
(5.6) |
385 |
(43.5) |
180 |
(20.3) |
|
3/0–4/0 |
85.0–107.2 |
– |
– |
50 |
(5.6) |
500 |
(56.5) |
250 |
(28.2) |
|
250–350 |
(127–177) |
– |
– |
50 |
(5.6) |
650 |
(73.4) |
325 |
(36.7) |
|
400 |
(203) |
– |
– |
50 |
(5.6) |
825 |
(93.2) |
375 |
(36.7) |
|
500 |
(253) |
– |
– |
50 |
(5.6) |
825 |
(93.2) |
375 |
(42.4) |
|
600–750 |
(304–380) |
– |
– |
50 |
(5.6) |
1000 |
(113.0) |
375 |
(42.4) |
|
800–1000 |
(406–508) |
– |
– |
50 |
(5.6) |
1100 |
(124.3) |
500 |
(56.5) |
|
1250–2000 |
(635–1010) |
– |
– |
– |
– |
1100 |
(124.3) |
500 |
(67.8) |
Inside Hex Screws — Tightening Torque Values
|
Socket size across flats |
Torque Value |
||
|---|---|---|---|
|
Inches |
(mm) |
lb-in. |
(N•m) |
|
1/8 |
(3.2) |
45 |
(5.1) |
|
5/32 |
(4.0) |
100 |
(11.3) |
|
3/16 |
(4.8) |
120 |
(13.6) |
|
7/32 |
(5.6) |
150 |
(16.9) |
|
1/4 |
(6.4) |
200 |
(22.6) |
|
5/16 |
(7.9) |
275 |
(31.1) |
|
3/8 |
(9.5) |
275 |
(42.4) |
|
1/2 |
(12.7) |
500 |
(56.5) |
|
9/16 |
(14.3) |
600 |
(67.8) |
Ground Bus Connections
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
The ground bus is bolted to the frame near the bottom of the equipment. It is arranged so that connectors to the station ground can be made in any unit. If the equipment is shipped in more than one group, connect the sections of the ground bus by using the splice plates provided with the equipment. Assemble joints as described in Bus Connections.
Ground bus connections are made in the lower portion of the cable entrance compartment. Connect the ground bus to the station ground bus using a conductor with a current-carrying capacity equal to that of the ground bus.
Fuse Installation
The fuses provided by Schneider Electric should be installed following the equipment installation process. The installer is responsible for the proper installation of fuses, holders, fittings, etc.
DANGER |
|---|
|
HaZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Do not perform fuse installation or replacement on energized
equipment.
Failure to follow these instructions will result in death or serious injury.
|
-
Verify that all fuses, holders, etc. are correctly installed and secured.
-
Verify that all fuses are latched/locked in place if latching/locking style fuses are provided.
Refer to the relevant fuse instruction manuals for detailed assembly and installation instructions.
Interlocks
Interlocks should be checked for proper operation before power is applied to the motor controller equipment. Check the access interlock to verify that:
-
The power fuses cannot be accessed unless the disconnector switch is open.
-
The disconnector switch cannot be closed while the power fuses are accessible.
DANGER |
|---|
|
HaZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Before placing the equipment into operation, see Operation, and consult the drawings for proper operating sequence.
The load break interrupter switch is equipped with a mechanical device that blocks access to a closed switch. In addition, the load break interrupter switch must be opened before the medium voltage door can be opened.
High Potential (Hi-Pot) Testing
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
Power Circuit
Perform a one-minute power frequency voltage withstand test, commonly referred to as a high potential (hi-pot) test, to measure insulation integrity of the power circuit. Refer to the table Hi-Pot Field Test Values for test values and additional information.
WARNING |
|---|
|
Overvoltage to control and protective components
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Take the following steps to help promote the safety of personnel and equipment:
-
Restrict entry into the area to prevent any unauthorized personnel from approaching the gear during testing.
-
Notify all persons that the test is going to be conducted.
-
Follow all local lockout and tag-out procedures.
-
Disconnect surge arresters, surge capacitors, and power factor correction capacitors (if supplied).
-
Disconnect or ground capacitive dividers, if supplied.
-
Do not use unfiltered, half-wave rectified DC hi-pot test units. Use of such devices greatly increases the chance of x-ray generation.
-
Ground control side of circuit or disconnect control components that could be damaged during hi-pot testing. Refer to the job drawings.
Hi-Pot Field Test Values
| Equipment Maximum Rating (kV) | Field Test Values | |
|---|---|---|
| AC (kV) | DC (kV) | |
|
2.4 |
5.5 |
7.9 |
|
3.3 |
7.1 |
10.1 |
|
4.16 |
8.5 |
12.1 |
|
4.8 |
9.6 |
13.6 |
|
5 |
10.0 |
14.1 |
|
5.5 |
10.8 |
15.3 |
|
6 |
11.6 |
16.4 |
|
6.6 |
12.7 |
17.9 |
|
6.9 |
13.2 |
18.7 |
Phase-to-Phase Hi-Pot Testing
Follow these steps to perform a phase-to-phase hi-pot test:
-
Gradually increase the voltage to the levels shown in the table Hi-Pot Field Test Values for test values and additional information.
-
Verify that the equipment sustains the specified voltage without flashover for one minute.
-
Turn off the test equipment. Discharge high potential test cables to ground before removing the test cables.
Phase-to-Ground Hi-Pot Testing
Follow these steps to perform a phase-to-ground hi-pot test:
-
Gradually increase the voltage to the levels shown in the table Hi-Pot Field Test Values for test values and additional information.
-
Verify that the equipment sustains the specified voltage without flashover for one minute.
-
Turn off the test equipment. Discharge high potential test cables to ground before removing the test cables.
If the test is unsuccessful, inspect the insulators for leakage paths. If necessary, clean the surface of the insulator(s) with denatured alcohol and re-test. If problems persist, DO NOT ENERGIZE THE EQUIPMENT. Contact your local field sales office or your distributor.
If the equipment has been stored for several months or has been exposed to high humidity during the storage time period, perform a hi-pot test. First energize the heater circuits for a minimum of 24 hours. See the table Hi-Pot Field Test Values for test values and additional information. Follow other equipment testing procedures as required by customer in-house standards.
Control Circuit
| NOTICE |
|---|
|
overvoltage to control and protective components
Failure to follow these instructions can result in equipment damage.
|
Control Circuit-to-Ground Hi-Pot Testing
Follow these steps to perform a control circuit-to-ground hi-pot test:
-
Gradually increase the voltage to the appropriate test level based on the equipment’s control voltage.
-
Verify that the equipment sustains the specified voltage without flashover for one minute.
-
Turn off the test equipment. Discharge high potential test cables to ground before removing the test cables.
Performing a Final Inspection
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
After installing the equipment and making all interconnections, follow these steps to test the equipment and perform a final inspection before placing it in service:
- Verify that a hi-pot test has been performed.
- Check all control wiring with the wiring diagrams.
- Verify that all connections are properly made and tightened.
- Verify that all fuses are installed,
- Verify that current transformer circuits are complete.
- Verify that all event detection devices have been properly connected and set.
- Verify that loose connections are tightened to the proper tightening torque (see Slotted Screws and Hex Bolts — Tightening Torque Values and Inside Hex Screws — Tightening Torque Values).
- Verify that all protective relays have been configured
with proper settings per the outcome of the customer’s coordination
study.
- The contactor opening time must be coordinated with the supplied power fuse's time-current characteristics.
- Power fuses must interrupt currents which exceed contactor ratings.
- Ensure that all transition, control, and timing relays are configured per application requirements.
- Verify that all insulating surfaces, including the primary support insulators and isolation barriers, are clean and dry.
- Verify that all fuses are installed and orientated properly and do not exceed the nameplate rating for their sections.
- Before energizing any source of electric power, make a final check of the equipment. Inspect every compartment for loose parts, tools, litter, and miscellaneous construction items.
- Review key interlock schemes carefully (if used). Insert only the proper keys in the locks. Remove all extra keys and store them where only authorized personnel can access them.
- Verify that all barriers, covers, and doors are secured.
DANGER
WARNING