PKR8059601

Ratings

The following ratings apply to switches and equipment with stored energy-operated switches.

Indoor air interrupter switch ratings

System rating kV

Nominal kV rms

Max design kV rms

1.2 x 50 impulse withstand peak, kV

Cont. Amp., rms

Load switching Amp. rms

Mom. Amp., rms, asym.

2-second A, rms

Fault close A, rms, asym.

5

4.16

4.76

60

600

400

22500

14000

22500

7.2

6.9

8.25

95

600

400

22500

14000

22500

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?