Troubleshooting
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
For detail information about operation, troubleshooting, and maintenance requirements for the disconnector switch module, see the disconnector switch module manual.
Troubleshooting — High Voltage Fuses and Disconnect Switches
|
Problem |
Probable Cause |
Action |
|---|---|---|
|
Overheating |
Overload |
If the excess current causes the switch to overheat, either:
|
|
Poor contact (contact out of alignment) |
Adjust contacts. |
|
|
Connections to switch: inadequate current-carrying capacity |
Increase the capacity of the connections by adding conductors or by replacing with heavier conductors. |
|
|
Contact burned or pitted |
Dress and fit the contacts properly. |
|
|
The bolts and nuts on the connections are not tight |
Tighten all bolts and nuts. NOTE: Do not apply too
much pressure when tightening the nuts on bolts. Using a wrench that
is too large can further loosen the connection by causing the bolts
to expand beyond their elastic limit. See Bolt Torque Values for Bus Connections.
|
|
|
Ambient temperature too high (too close to a boiler, a furnace, etc.) |
Relocate to the equipment to a cooler place or implement cooling methods. |
DANGER