PKR8059601

About This Document

Document Scope

Use this document to:

  • Install, operate, maintain, and troubleshoot the MotorSeT™ Load Break Interrupter Switch 400 A, 5 kV.

Validity Note

This instruction bulletin is valid for MotorSeT Load Break Interrupter Switch 400 A, 5 kV installations in the North American region only. Visit the Schneider Electric website (www.se.com) for additional information regarding this offer.

NOTE: This equipment is certified to Underwriters Laboratories Inc., standard UL 347. For regions outside of North America, consult your local and national standards to determine if and how they differ from UL 347.

For product compliance with environmental directives such as RoHS, REACH, PEP, and EOLI, go to www.se.com/green-premium.

For technical characteristics of the physical modules described in this bulletin, go to www.se.com.

The technical characteristics presented in this bulletin should be the same as those that appear online. The content may be revised over time to improve clarity and accuracy. If there is a difference between the information contained in this bulletin and online information, use the online information.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?