Maintenance
Read and understand the following precautions before performing any maintenance. See Requirements for Installation, Operation, and Maintenance for additional information.
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Regular Inspections
Regular Inspections Frequency
|
Environmental Conditions |
Inspection Frequency |
|---|---|
|
Normal conditions, such as:
|
Every year |
|
Harsh conditions, such as:
|
Every three months |
Cleaning the Switch Components
All switch components, including insulators and blade assemblies must be cleaned as follows:
-
Every year or after 1000 operations
-
Wipe the dust from the components with a clean dry cloth. After cleaning, apply a light coat of non-corrosive high-temperature grease that will not harden upon exposure to air (SHC-32 Mobiltemp or equivalent) to all contact surfaces.
Contact Inspection
Check the blades and ensure that they are making good contact.
-
Conduct a contact resistance measurement between (1) the jaw and spade terminal and (2) the hinge spade terminals. It should read less than 80 micro-ohms.
-
Ensure that the blades can be "opened" from the jaw casting with a pulling force of 8–10 pounds measured at the aluminum spacer between the main blades.
-
Wipe and clean the contacts, especially if the switch has not been in operation for a while. Open and close the switch several times in succession to do so.
CAUTION |
|---|
|
Switch blade contact Damage
Do not clean the blades with abrasive materials or abrasive
cleaners.
Failure to follow these instructions can result in injury or equipment damage.
|
Insulators
Keep all insulator surfaces clean, particularly when the switches are in harsh environmental conditions. Clean the insulators with a clean lint-free cloth dampened with either denatured alcohol or isopropyl alcohol.
Carefully inspect all insulators for signs of carbon tracking. Focus on areas where the conductor passes through an insulator or are near a barrier. Examine the surface for cracks or discoloration. Contact your Schneider Electric field sales representative if any of these conditions exist.
Bus and Conductor (Switch Blade)
Inspect the bus and connections for evidence of overheating or damage.
-
Using an appropriate insulation tester or Megger™, measure and record the resistance to ground, and the resistance between phases of the bus and connections insulation.
-
Measure and record the ambient temperature and humidity.
Analyze these readings over consecutive periods to identify trends indicating insulation degradation.
Operating Shaft
The operating shaft connects the stored energy mechanism to the switch operating arm. Lightly coat the shaft bearings, door interlocks, and door latch surfaces with lubricant (white lithium grease).
Push Rods
Each main blade in the switch is connected to the main operating shaft by an insulating pushrod. Check the pushrods for signs of damage to either end each time a normal maintenance inspection is performed.
Stored Energy Mechanism
The moving parts are the front and rear latches, which are spring-operated, and the two shaft bearings. Check the moving parts after approximately 100 operations to make sure the latches rotate freely up and down using finger pressure on the rollers. Check for loose bearing bolts.
Lubrication
Mechanical (non-electrical contacts): Clean and lubricate the bearing points and sliding surfaces at regular intervals with a thin film of white lithium grease. Before lubrication, remove any hardened grease and dirt from the latch and bearing surfaces with a clean, dry lint-free cloth.
Disconnector switch contacts: Clean and grease the contact surface of the movable blades and the stationary contact surfaces with SCH-32 Mobiltemp, or equivalent.
High Potential Tests
Perform a one minute high potential test on the primary circuit, busing and interrupter switch, at a field test value of either 14 kV AC or 20 kV DC.
Maintenance Checklist
The following tables list the inspection checks that are necessary to maintain and to verify that the equipment remains operational.
Cable and Bus Checklist
| Inspect bolts on bus connections for tightness | |
| Check clearance phase-to-phase and phase-to-ground of cable and bus. | |
| Check the bus and cable supports to verify they are adequate. | |
| Inspect the cables for insulation damage and broken conductor strands near the cable lug. | |
| Inspect the cable termination in the cable lugs for tightness. | |
| Inspect the placement of phase markings. | |
| Check the plating on busbars. | |
| Inspect the taped joints for tightness (when applicable). | |
| Check the connections on the lugs. | |
| Inspect the taped joints for coverage of insulating varnish and heating. |
Key Interlocks Checklist
| Check the door block for lubrication. | |
| Check the key interlock system for appropriate sequence and operation. | |
| Verify that the interlock is free from binding. | |
| Check to verify the weather cap fits securely (outdoor only). | |
| Ensure that the key nameplate matches the key number. | |
| Check to verify that the handle stops on casting do not interfere with the interlock mechanism. | |
| Remove all spare keys. |
Fuse Accessories Checklist
| Check contact of fuses mounted in the fuse clip. | |
| Inspect the unit for spare fuse holder or mounting. | |
| Check the alignment of fuses with the fuse clips. |
Unit General Misc. Checklist
| Inspect the phase barriers for proper mounting. | |
| Check the unit for nomenclature and manufacturer's nameplates. | |
| Inspect the paint coverage of unit. | |
| Inspect the door handles, locking bars and mechanism and lubricate. | |
| Inspect for damaged, bent, or twisted doors. | |
| Check the unit for proper device markings. | |
| Inspect the unit for gasketed joints (outdoor only). | |
| Check the unit for water tightness, dirt, moisture, and rust. | |
| Inspect the unit for door stop alignment (when applicable). | |
| Inspect the unit doors for adequate opening. | |
| Check the louvers (if applicable) for proper backup and clean filters. | |
| Seal all non-ventilation openings to help prevent moisture, vermin, rodents, snakes, etc. from entering the equipment. | |
| Check the insulator for heat. | |
| Check and torque all bolts. | |
| Check the heaters, thermostats, and other environmental controls. |
DANGER
CAUTION