Operation
See also, Requirements for Installation, Operation, and Maintenance for additional information.
Load Break Interrupter Switch 400 A, 5 kV
The MotorSeT Load Break Interrupter Switch 400 A, 5 kV has spring mechanisms that provide quick "make" (rated fault closing) and quick "break" (rated load interruption) operation.
As the operator handle is rotated, the charged spring is driven off-center and releases its energy, thereby rotating the operating shaft. The switch blades will not move, in either a closing or opening direction, until the main spring causes rotation of the operating shaft.
The load break interrupter switch has several built-in features:
-
A door interlock that blocks opening the enclosure's front door while the switch is in the closed position
-
A switch interlock that blocks manual operation of the handle mechanism while the door is open
-
A viewing window to view each switch contact position
-
Capability for padlocking the switch in the Off/Open position
-
Capability for padlocking the door handles closed
-
Mechanical indicators showing whether the switch is open or closed
-
Key interlocks (when provided) force a sequence of operation
Disconnector Switch Operation
Opening the Disconnector Switch
To open the disconnector switch, follow these steps:
-
If the controller is supplying power to the motor, press the Stop button on the control panel to remove power to the motor.
-
Grasp the disconnector switch operator handle and rotate the handle counter-clockwise downward to the Off/Open position (shown in Handle Positions).
-
Use the viewing window to view the disconnector switch and verify that the disconnector switch is in the Off/Open position.
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
Closing the Disconnector Switch
To close the disconnector switch, follow these steps:
-
Use the viewing window to view the disconnector switch and verify that the disconnector switch is in the Off/Open position (shown in Handle in Off/Open Position) .
-
Grasp disconnector switch operator handle and rotate the handle clockwise upward to the On/Closed position (shown in Switch Handle On/Closed Position).
-
Use the viewing window to view the disconnector switch and verify that the blades for all three phases are in the On/Closed position (shown in Switch Blades in Closed Position).
DANGER