Influence of Harmonics on Aging
Harmonics
|
Influence |
Appearance |
Consequences |
|---|---|---|
|
Increase in skin effect, proximity effect, iron loss, Foucault/Eddy currents |
|
Harmonics cause temperature rise greater than that of the fundamental current |
|
Possible overload of neutral if third-order harmonics and their multiples are present |
Distorted waveform |
|
Recommendations
The maintenance and installation recommendations according to the harmonics are defined in the following table:
|
THDi in % of In |
Description |
Maintenance recommendations |
Installation recommendations |
|---|---|---|---|
|
≤ 30 % |
No notable influence on aging. |
Implement the Intermediate program. |
No particular recommendation |
|
30 % to 50 % |
At 40 % THDI, potential heat generation is approximately 10 % higher, corresponding to 5 % more current. |
Carry out more frequent periodic checks. |
Standard filtering with an inductor to reduce harmonics |
|
> 50 % |
– |
Carry out more frequent periodic checks. |
If necessary:
|