DOCA0099EN-05

How to Maintain Mechanical Interlocking Systems

@TW: profiled topic used in Maintenance Guides: DOCA0305 (MTZ with Mic Act), DOCA0099 (MTZ with Mic X), LVPED508016 (NT/NW)

Functions

A source changeover system, either manual or automatic (ATS), enhances the continuity of service of an electrical distribution system.

Mechanical interlocking between the devices in the source changeover system prevents the closing of two devices simultaneously.

The use of mechanical interlocking for source-changeover systems using cables or connecting rods is compulsory for Automatic Transfer Switch (ATS) applications.

A mechanical interlocking system is made of the following parts depending on the type of MasterPacT MTZ devices:

  • An interlocking plate on the side of each MasterPacT MTZ device.

  • A set of cables or connecting rods linking the MasterPacT MTZ devices.

The figure below illustrates a mechanical interlocking system by cable for source changeover between two MasterPacT MTZ2 devices:

Degradation Factors

The factors which can cause degradation of the mechanical interlocking system are the following:

  • Dusty or dirty environment

  • Vibration

Potential Hazards

Performing regular maintenance on the mechanical interlocking system can help to avoid the potential hazards and consequences listed in the following table.

Hazard

Consequence

Personal injury

Equipment damage

Inappropriate or no operation of the source changeover system

Death or serious injury

Preventive Action

The following table lists the preventive maintenance procedures to be performed to maintain the mechanical interlocking system.

Maintenance program

Preventive action

Procedure

Routine end-user preventive maintenance

Operate interlocking systems

Mechanical Interlocking NII_Z_1

Manufacturer preventive maintenance

Operate mechanical interlocking by cable.

Contact your Schneider Electric Services representative.

Operate mechanical interlocking by rod.

For more information, refer to Preventive Maintenance Programs.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.