Influence of Dust on Aging
Dust
|
Influence |
Appearance |
Consequences |
|---|---|---|
|
Deposit on grease of mechanisms (device and chassis) |
Change in color and texture of greases |
|
|
Deposit on grease of clusters |
Change in color and texture of greases |
|
|
Deposit on displays |
– |
Screen data not legible |
|
Deposit on insulation |
– |
|
|
Deposit on device contacts |
– |
Increased contact resistance and temperature rise |
Recommendations
The maintenance and installation recommendations according to the dust levels are defined in the following table:
|
Dust deposit |
Description |
Maintenance recommendations |
Installation recommendations |
|---|---|---|---|
|
Low level |
Quantity of dust generally deposited on and around devices in commercial buildings and on standard industrial premises |
|
Switchboard with standard IP |
|
Moderate level |
Quantity of dust deposited on and around devices inside switchboards equipped with filters or a ventilated IP54 enclosure, and installed in dusty environments (for example, cement works, grain mills, incineration installations, plastic and steel mills, and mines) |
Carry out more frequent periodic cleaning. |
Make sure that the switchboard remains closed. |
|
High level |
Quantity of dust deposited on and around devices inside switchboards without filters or without ventilated IP54 enclosure, and installed in dusty environments (for example, cement works, grain mills, incineration installations, plastic and steel mills, and mines) |
Carry out more frequent periodic cleaning. |
It is mandatory to install the switchgear in special equipment offering protection against dust. |