Manufacturer Preventive Maintenance Program
Definition
The Manufacturer preventive maintenance program must be done exclusively bySchneider Electric Services representatives.
The Manufacturer preventive maintenance program includes the Routine and Intermediate end-user preventive maintenance programs.
The Manufacturer preventive maintenance program comprises:
-
Complete function checks.
-
Condition checks (test-based).
-
Complete part and system servicing (cleaning, greasing).
-
Control unit replacement (diagnostic-based).
The Manufacturer preventive maintenance program must be performed every five years in the case of normal operating conditions and user application with low criticality. Refer to the recommended frequency for the Manufacturer maintenance program for other cases.
Procedures
|
Part |
Procedure title |
|---|---|
|
Device |
Measure insulation resistance |
|
Mechanism |
Check opening and closing forces |
|
Clean and regrease the mechanism |
|
|
Breaking unit |
Measure the contact resistance for each pole |
|
Auxiliaries |
Check opening time of MX opening voltage release |
|
Check closing time of XF closing voltage release |
|
|
Check opening time of MN undervoltage release |
|
|
Preventively replace the XF, MX, MN voltage releases (1) |
|
|
Preventively replace MicroLogic X control unit and electrronic modules |
|
|
Control unit |
Diagnose the performance of the MicroLogic X control unit functions |
|
Preventively replace the MicroLogic X control unit (2) |
|
|
Chassis |
Check connection/disconnection torque |
|
Clean and regrease chassis of MasterPacT drawout devices |
|
|
Communication system |
Check data transmission over the IFE Ethernet interface or EIFE embedded Ethernet interface |
|
Mechanical interlocking |
Operate mechanical interlocking by cable |
|
Operate mechanical interlocking by rod |
|
|
(1) As part of the preventive maintenance plan, Schneider Electric recommends replacing the voltage releases after 15 years of operation. (2) As part of the preventive maintenance plan, Schneider Electric recommends that the Schneider Electric Services representative replaces the MicroLogic X control unit and associated optional ESM or M2C modules after 15 years of operation. Each time the MicroLogic X control unit is replaced, the performer, and the rating and sensor plugs must be replaced by theSchneider Electric Services representative. |
|
Time Required
The average total time required for a Schneider Electric Services representative to perform this maintenance program including the Intermediate one, is as follows:
-
From 1.5 hours to 2 hours depending on the frame size, for a fixed device with all accessories installed.
-
From 2 hours to 3 hours depending on the frame size, for a drawout device with all accessories installed.