How to Maintain the Communication System
Functions
The communication system allows data transmission between the device and the remote controller. It can be used to remotely operate (open/close) the device.
Maintenance, production, management, and other departments can use this function to manage energy and assets, and monitor the quality of the electrical network.
In MasterPacT MTZ circuit breakers, the device data can be accessed by using the ULP port module connected to a communication interface and an appropriate software tool such as EcoStruxure Power Commission software.
Degradation Factors
The factors which can cause degradation of the communication system are the following:
-
Vibration
-
Electro-magnetic field disturbances
-
Equipment and software breakdown
-
Modification of communication system architecture
Potential Hazards
Performing regular maintenance on the communication system can help to avoid the potential hazards and consequences listed in the following table.
|
Hazard |
Consequence |
|
|---|---|---|
|
Personal injury |
Equipment damage |
|
|
Incorrect or no operation (critical to safety) as a result of misleading information |
Death or serious injury |
– |
|
Communication loss |
– |
Inappropriate functioning of devices, communication interfaces or modules on communication network |
|
Incorrect decision taken as a result of misleading information (status, metering, health) |
– |
Inappropriate functioning of devices, communication interfaces or modules on communication network |
|
Incorrect system management leading to financial losses |
– |
Inappropriate functioning of devices, communication interfaces or modules on communication network |
Preventive Action
The following table lists the preventive maintenance procedures to be performed to maintain the communication system.
|
Maintenance program |
Preventive action |
Procedure |
|---|---|---|
|
Manufacturer preventive maintenance |
Check data transmission over the IFE Ethernet interface or EIFE embedded Ethernet interface. |
Contact your Schneider Electric Services representative. |
For more information, refer to Preventive Maintenance Programs.