Influence of Load on Aging
Percent Load (I/In)
The percent load affects the device temperature, which is itself affected by the ambient temperature.
|
Influence |
Appearance |
Consequences |
||
|---|---|---|---|---|
|
Aging of plastic insulation |
Change in color of insulation |
Breaking of parts leading to potential failure of functions. |
||
|
Aging of grease |
Change in color and viscosity |
Increase in mechanical friction. |
||
|
Aging of electronic components |
Modified display of LCDs |
A 10 °C (50 °F) increase (that is, an 85 % load) reduces the service life of components by approximately half. |
||
|
Deterioration of characteristics:
|
Rupture |
Non-operation of mechanisms. |
||
Recommendations
The maintenance and installation recommendations according to the value of percent load (I/In) are defined in the following table:
|
Percent load |
Description |
Maintenance recommendations |
Installation recommendations |
|---|---|---|---|
|
I/In ≤ 80 %, 24/24 h |
Maximum percent load taken into account in sizing the installation. At this percent load, temperature rise is reduced approximately 40 % with respect to a 100 % load. |
Implement the Intermediate program. |
Normal conditions |
|
I/In ≤ 90 %, 8/24 h |
At this percent load, temperature rise is reduced only 20 %. Heating and cooling cycles impact on the mechanical junctions of the power circuit. |
Carry out more frequent periodic checks. |
Normal conditions |
|
I/In ≤90 %, 24/24 h |
The thermal stress for continuous operation is three times higher than in the previous case, but the absence of thermal cycles slows aging of the electromechanical components. |
Preventive maintenance is difficult due to the continuous process |
Normal conditions |
|
I/In = 100 %, 8/24 h |
Between 90 % and 100 %, temperature rise is close to its maximum value. Heating and cooling cycles impact on the mechanical junctions of the power circuit, with major impact on aging. |
|
|
|
I/In = 100 %, 24/24 h |
Between 90 % and 100 %, temperature rise is close to its maximum value. This situation has a major impact on aging. It is not recommended. |
|
|