How to Maintain the Case
Functions
The case of the device:
-
Insulates the main contacts
-
Helps to protect the user against arcing effects
-
Provides a support for:
-
Mechanism
-
Control unit
-
Auxiliaries
-
Power connection
-
-
Withstands the thermal and electrodynamic stresses generated during short-circuits
Degradation Factors
The factors which can cause degradation of the case are the following:
-
Dusty or dirty environment
-
Humidity
-
High ambient temperature
-
Shocks
-
Stresses due to high short-circuit currents
Potential Hazards
Performing regular maintenance on the case can help to avoid the potential hazards and consequences listed in the following table.
Hazard |
Consequence |
|
---|---|---|
Personal injury |
Equipment damage |
|
Arc flash |
Death or serious injury |
– |
Insulation resistance of the case too low and impulse voltage |
Electric shock |
– |
Disruptive discharge |
– |
Degradation of the breaking unit |
High short-circuit current |
– |
Degradation of the breaking unit |
Preventive Action
The following table lists the preventive maintenance procedures to be performed to maintain the case of the device.
Maintenance program |
Preventive action |
Procedure |
---|---|---|
Routine end-user preventive maintenance |
Check the general condition of the device. |
Device NII_Z_1 |
Manufacturer preventive maintenance |
Measure the insulation resistance. |
Contact your Schneider Electric Services representative. |
For more information, refer to Preventive Maintenance Programs.