Influence of Corrosive Atmosphere on Aging
Corrosive Atmosphere
Corrosive atmosphere |
Influence |
Appearance |
Consequences |
Thresholds per class in ppm (1) |
---|---|---|---|---|
SO2 Sulphur dioxide |
Corrosion of silver, aluminum, and bare copper Phenomenon accelerated by high temperature and relative humidity. |
|
|
|
H2S Hydrogen sulphide |
Sulphurization of silver. Phenomenon accelerated by high temperatures. |
|
|
|
Cl2 Chlorine |
Corrosion of metal parts |
|
|
|
NH3 Ammoniac |
|
|
|
|
NO2 Nitrogen oxide |
Corrosion of metal parts |
Oxidation |
Increased temperature rise |
|
Oily atmospheres |
Attacks polycarbonates |
Cracking of polycarbonates |
|
– |
(1) ppm = parts per million in volume |
Recommendations
The maintenance and installation recommendations according to the environment categories as per IEC 60721-3 standard are defined in the following table:
Class |
Zone |
Presence of corrosive gases |
Impact on device |
Maintenance recommendations |
Installation recommendations |
---|---|---|---|---|---|
3C1 |
Rural zones or urban zones with low industrial activity |
Negligible |
No impact on service life because concentrations are very low. |
Implement the Intermediate program. |
No particular recommendation |
3C2 |
Urban zones with scattered industrial activity and heavy traffic |
Low level |
Moderate impact on service life. |
Implement the Intermediate program. |
No particular recommendation |
3C3 |
Immediate vicinity of industrial pollution Example: paper mills, water treatment, chemicals, synthetic fibers, smelting plants |
Significant level |
|
Implement the Intermediate program. |
No particular recommendation |
3C4 |
Inside polluting industrial premises Example: paper mills, water treatment, chemicals, synthetic fibers, smelting plants |
High level |
|
|
|