General Information

General Instructions

The special feature options covered in this Panelboard estimating procedure are applicable to factory-assembled panelboards only. Do not apply this pricing to ready-to-assemble panelboards.

Special features are listed in three major categories:

  • Mains

  • Branches

  • Cabinets


Metric Conversion

Inches (in.) x 25.4 = millimeters (mm).


I-Line™ Panelboards Factory Assembled

Panel Type

No.

Poles

Main Circuit Breaker

400 A

600 A

LX[1]

LE[1]

LXI [1]

LX[1]

LE[1]

LXI[1]

HCP, HCP-SU

2

           

3

           

Footnotes

  1. Std. construction back-fed main.
Feedback