Retrofit Existing Enclosure Data Sheet

Data Sheet for Panelboards to Retrofit Existing Enclosures

Distributor:

 

Job Name:

 

Contractor:

 

Panel Marking:

 

The following dimensions are necessary for quotation and production of a panel to fit an existing enclosure. Provide dimensions in inches only.

Existing Flush-Mounted Enclosures

  • Height dimension “A”:

  • Width dimension “B”:

  • Depth dimension “C”:

  • Flange width dimension “D”:

  • If enclosure is not flush with Plaster Line, dimension “E”:

    Existing Surface-Mounted Enclosures

  • Height dimension “A”:

  • Width dimension “B”:

  • Depth dimension “C”:

  • Flange dimension may be either dimension “D” or “F”
    (select one)

    • Dimension “D”:

    • Dimension “F”:

      note

      Trims are furnished so that the interior must be centered within the enclosure.

      If the enclosure is deeper than the standard panelboard enclosure for the required type of panelboard, customer-supplied mounting brackets may be necessary to bring the interior out to the front of the enclosure.

      If interior requires a vented enclosure, contact your nearest Schneider Electric sales office for assistance.

Feedback