the servo drives and servo motors provides maximum power in the minimum space, which helps to reduce overall machine size and costs. The ability to use 3rd party motors, multiple communication cards, as well as standard encoders, enable adaptation to numerous types of control system architecture for
contactors, reversing contactors, reversing Each 3-pole device is pre-wired with line and load side power wiring for reversing applications. Each 4-pole device is prewired with load side power wiring. TeSys Deca Mechanically-Interlocked Reversing Contactors Maximum Horsepower Ratings Maximum Current
sealed logic reed Hermetically Sealed Power Reed Contact Blocks Hermetically Sealed Power Reed Contact Blocks contact blocks hermetically sealed power reed Type K, SK and KX Contact Block “H” Numbers Type K, SK and KX Contact Block “H” Numbers Class 9001 / Refer to Catalog 9001CT1103 Class 9001 / Refer