TeSys DF Fuseholders

Refer to Catalog 9080CT1301

Modular Fuseholders

DFCC1

DFCC2V

Modular Fuse Holders, TeSys DF [1]

Rated
Thermal Current

Type
of Fuse

Composition

Blown Fuse
Indicator

Standard Pack
Quantity

Catalog
Number

30 A

Class CC

1 Pole

No

1 Pole

DFCC1

Yes

DFCC1V

2 Pole

No

2 Pole

DFCC2

Yes

DFCC2V

3 Pole

No

3 Pole

DFCC3

Yes

DFCC3V

File: E310269, CCN: IZLT

   

Also see TeSys DF and LS1 Fuse Carriers on www.se.com/us

Footnotes

  1. For additional fuse holders and information, refer to Catalog 9080CT0801.
Feedback