DOCA0133EN-01

DPST

double-pole/single-throw. A switch that connects or disconnects 2 circuit conductors in a single branch circuit. A DPST switch has 4 terminals, and is the equivalent of 2 single-pole/single-throw switches controlled by a single mechanism, as depicted below:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?