DOCA0133EN-01

TCC

trip curve characteristic. The type of delay used to trip the flow of current in response to a trip condition. As implemented in the LTM R controller, all motor protection function trip time delays are definite time, except for the Thermal Overload function, which also offers inverse thermal trip time delays.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?