DOCA0133EN-01

FLC

full load current. Also known as rated current. The current the motor will draw at the rated voltage and rated load. The LTM R controller has 2 FLC settings: FLC1 (Motor Full Load Current Ratio) and FLC2 (Motor High Speed Full Load Current Ratio), each set as a percentage of FLC max.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?