DOCA0133EN-01

RTD

resistance temperature detector. A thermistor (thermal resistor sensor) used to measure the temperature of the motor. Required by the LTM R controller’s Motor Temp Sensor motor protection function.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?