DOCA0279EN-02

Compatibility

The following table shows the compatibility of digital tools with the TeSys Tera system in active releases.

Configuration or Programming software   TeSys Tera firmware version

TeSys Tera DTM

DTM v2.0.1

  • TeSys Tera_Serial_V002.000.000.sedp

    (The analog I/O module is not supported in this version)

  • TeSys Tera_Serial_V002.001.002.sedp
  • (The analog I/O module is supported in this version)
   
  • TeSys Tera_Ethernet_V001.000.003.sedp

  • TeSys Tera_Ethernet_V001.000.004.sedp

For more information about firmware update procedure, refer to TeSys Tera Motor Management System DTM Library Online Help Guide – DOCA0275EN.

NOTE: For TeSys Tera Ethernet, Firmware versions TeSys Tera_Ethernet_V001.000.000.sedp or TeSys Tera_Ethernet_V001.000.001.sedp require a mandatory update to version TeSys Tera_Ethernet_V001.000.003.sedp
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.