DOCA0279EN-02

Introduction

The TeSys Tera system is designed as a reliable building block for Intelligent Motor Control Centres (iMCCs) to provide complete protection, metering, control, and monitoring capabilities for single-phase or three-phase AC induction motors. The system is installed in the low voltage switchgear system and connects the higher level automation system through fieldbus network and the motor feeder.

A LTMTCT/LTMTCTV sensor module
B LTMT main unit
C Start/Stop commands
D LTMT expansion modules
E

PC running SoMove FDT container software with TeSys Tera DTM installed and equipped with standard web server capability

F

Programmable Logic Controller (PLC) or Distributed Control System (DCS)

G Ethernet switch
H LTMTCUF control operator unit

For more information, refer to TeSys Tera Motor Management System User Guide – DOCA0257EN.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.