DOCA0279EN-02

TeSys Tera DTM Library Update Policy

The TeSys Tera DTM Library update is recommended to benefit from the latest features and potential bug fixes.

NOTE: It is recommended not to update the TeSys Tera DTM Library to the latest version, if the latest features are not required for your application and no bug fixes are provided.

Use this release note to determine whether an update to the latest version of the TeSys Tera DTM Library is relevant for your application.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.