DOCA0279EN-02

Hardware Requirements

The following hardware requirements are recommended on the PC to install the TeSys Tera DTM Library.

Equipment

Minimum requirement

Recommended requirement

Processor

Pentium 4 or Core 2 Duo, 2 GHz

Intel® Core™ i3

RAM

2 GB

4 GB

Display

Resolution: 1024 x 768, 1366 x 768, 1600 x 1900, and 1920 x 1080 pixels

Resolution: 1600 x 1900 and 1920 x 1080 pixels

DPI: 96 (100%) and 120 (125%)

DPI: 96 (100%) and 120 (125%)

Free hard disk space on system drive

1 GB

2 GB

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.