DOCA0279EN-02

TeSys Tera DTM Library Versions

The following versions of the TeSys Tera DTM Library are applicable for:

  • LTMT main unit with Modbus RTU

  • LTMT main unit with PROFIBUS DP

  • LTMT main unit with EtherNet/IP

Version

Release

TeSys Tera DTM Library v2.0.1

Modbus RTU and PROFIBUS DP global release

TeSys Tera DTM Library v2.0.1

EtherNet/IP global release

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.