DOCA0279EN-02

DTM Overview

The DTM (Device Type Manager) is used together with FDT container (Field Device Tool container, also referred to as FDT frame) to commission and diagnose TeSys Tera system. The combination of FDT container and DTM is also called commissioning software.

Once a DTM is installed, it can be used by different FDT containers. For example, SoMove software (Schneider Electric).

For more information, refer to TeSys Tera Motor Management System User Guide – DOCA0257EN.

The TeSys Tera DTM Library configures the hardware during commissioning and topology management.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.