DOCA0278EN-00

Physical Device Replacement

Overview

This chapter provides information about the physical device replacement of TeSys T system to TeSys Tera system.

The physical marking of the terminals are available on all the modules of the TeSys T system and TeSys Tera system.

NOTE: The replacement of the TeSys T by the TeSys Tera has to be carried out only as a whole system and not as individual modules or devices.

For more details about the wiring and physical replacement or installation of the system, contact Schneider Electric or refer to TeSys Tera Motor Management System Installation Guide – DOCA0356EN.

For installation of the TeSys Tera system in an Okken switchboard, refer to Okken Communications Cabling and Wiring Guide (available on request).

For installation of the TeSys Tera system in a Blokset switchboard, refer to Blokset Communications Cabling and Wiring Guide (available on request).

NOTE: To obtain the above documents, contact Schneider Electric.

For installation of the TeSys Tera system in a Model 6 switchboard, refer to Model 6 Motor Control Centers Instruction Bulletin-80459-641-01 (available in Schneider Electric official website)

TeSys T to TeSys Tera Conversion:

Control Wiring

The following tables describe the terminal conversion from the TeSys T system to the TeSys Tera system.

Terminal Category

Legend

TeSys T

TeSys Tera

LTMR controller

LTMT main unit

Power supply

A

A1

A1

~/-

B

A2

A2

~/+

Digital Input Supply

WARNING
unintended machine operation
  • TeSys T digital inputs in the LTMRXFM series support 110-230  Vac and TeSys Tera LTMT main unit does not support 230 Vac digital inputs, it supports only 24 Vdc.
  • Use proper interposing relay between 230 Vac and 24 Vdc.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

@ Experts to confirm the terminal mapping

Terminal Category

Legend

TeSys T

TeSys Tera

LTMR controller

LTMT main unit

LTMT expansion module

LTMTIN42FM or LTMTIN42BD

Digital input

A

I.1

I.1

 

B

C

+24V

 

C

 

C

I.2

I.2

 

D

I.3

I.3

 

E

I.4

I.4

 

F

I.5

 

I.5

B

C

 

I.C

H

I.6

 

I.6

Terminal Category

Legend

TeSys T  
LTME expansion module

LTMT expansion module 1

LTMTIN42FM or LTMTIN42BD

LTMT expansion module 2

LTMTIN42FM or LTMTIN42BD

Digital input

A

I.7

I.7

 

B

C7

I.C

 

C8

 

C

I.8

I.8

 

D

I.9

 

I.5

E

C9

 

I.C

C10

 

F

I.10

 

I.6

Digital Ouput Supply

@Updated D4

Terminal Category

Legend

TeSys T

TeSys Tera

LTMR controller

LTMT main unit

LTMT expansion module

LTMTIN42FM or LTMTIN42BD

Digital output

A

13

O1

13

 

B

14

C1

14

 

B

24

C1

14

 

C

23

O2

23

 

D

33

 

O1

33

E

34

 

C1

34

F

95

NC

 

G

96

 

H

97

O3

C2

 

G

98

NO

 

Temperature Input Wiring

Terminal Category

Legend

TeSys T

TeSys Tera

LTMR controller

LTMT main unit

Temperature input

A

T1

T1

B

T2

T2

Communication Wiring

Terminal Category

Legend

Type of communication

TeSys T

TeSys Tera

LTMR controller

LTMT main unit

Communication

A

Modbus

D1

D1

B

D0

D0

C

S

Terminal Category

Legend

Type of communication

TeSys T

TeSys Tera

LTMR controller

LTMT main unit

Communication

A

PROFIBUS DP

S

B

A

A

C

B

B

NOTE: You can use side connector or sub-D9 connector for PROFIBUS DPcommunication. For more information, refer TeSys Tera Motor Management System PROFIBUS DP Communication Guide – DOCA0256EN.

Earth Leakage Wiring

Terminal Category

Legend

TeSys T  
LTMR controller

LTMTCT/LTMTCTV sensor module

Earth leakage

A

Z1

S1

B

Z2

S2

Voltage Input Wiring

Terminal Category

Legend

TeSys T

TeSys Tera

LTME expansion module

LTMTCT/LTMTCTV sensor module

Voltage input

A

LV1

L1

B

LV2

L2

C

LV3

L3

NOTE: The listed sensors are valid for use with the LTMTCTV••T or LTMTCTV••UT horizontal sensor module.

Cables

The following table describe the cables to be used for the migration from TeSys T system to TeSys Tera system:

@ Updated in Draft4

Legend

Connection to

TeSys T system TeSys Tera system

Description

Reference

Description

Reference

A

Sensor module

Connecting jumper 0.04 m (1.57 in.) length, for side by side connection of the LTMR and LTME

-

LTMT main unit to LTMTCT/LTMTCTV sensor module RJ11 connector cable 0.15 m (5.9 in) length.

LTMT9RJ1015

LTMT main unit to LTMTCT/LTMTCTV sensor module RJ11 connector cable 0.5 m (19.7 in) length.

LTMT9RJ105

LTMT main unit to LTMTCT/LTMTCTV sensor module RJ11 connector cable 0.2 m (7.87 in) length.

LTMT9RJ102

B

Expansion unit

LTMR to LTME RJ45 connector cable 0.3 m (11.81 in.) length

LTM9CEXP03

LTMT main unit to LTMT expansion module RJ45 connector cable 0.1 m (3.9 in) length.

LTMT expansion module to LTMT expansion module RJ45 connector cable 0.1 m (3.9 in) length.

LTMT9RJ401

LTMR to LTME RJ45 connector cable 1.0 m (3.28 ft) length

LTM9CEXP10

LTMT main unit to LTMT expansion module RJ45 connector cable 1 m (39.37 in) length.

LTMT9EX10

E

HMI

LTMT main unit to LTMTCUF control operator unit connection cable 1.0 m (39.3 in) length.

LTM9CU10S

LTMT main unit to LTMTCUF control operator unit connection cable 3.0 m (118.1 in) length.

LTM9CU30S

@ Updated in Draft4

The following table describe the common cables used in TeSys T system and TeSys Tera system:

Legend

Connection to

Description

Reference

C

PC

Cable kit, includes LTME/LTMR/LTMCU to PC communication cable 2.5 m (98.4 in) length

TCSMCNAM3M002P

D

EtherNet/IP network

Category 5 shielded/unshielded twisted-pair network connection cables with two RJ45 connectors

490 NTW 000 •••

Modbus RTU network

Modbus RTU network communication cable 0.3 m (11.81 in) length.

VW3A8306R03

Modbus RTU network communication cable 1.0 m (39.3 in) length.

VW3A8306R10

Modbus RTU network communication cable 3.0 m (118.1 in) length.

VW3A8306R30

PROFIBUS DP network

PROFIBUS DP network communication cable 100 m (328.08 ft) length.

TSXPBSCA100

PROFIBUS DP network communication cable 400 m (1,312.33 ft) length.

TSXPBSCA400

HMI Unit

The TeSys Tera system uses LTMTCUF control operator unit as the local HMI (Human Machine Interface).

NOTE:

The Control Operator Unit used in the TeSys T system is not compatible with the TeSys Tera system and should be replaced.

TeSys T system TeSys Tera system
Control operator unit Reference

LTMTCUF control operator unit

Reference

LTMCU (HMI device)

LTMCUF (HMI device with FDR service)

LTMTCUF

LTM9CU•0

(HMI communication cable)

TCSMCNAM3M002P

(cable kit)

LTM9KCU

(Kit for portable LTMCU)

Dimensions

Todo- Experts confirm the dimension
TeSys T system TeSys Tera system
LTMR controller

LTMT main unit with LTMTCT/LTMTCTV sensor module Front View

LTMT main unit with LTMTCT/LTMTCTV sensor module Side View

 
LTME expansion module

LTMT expansion module Front view

LTMT expansion module Side view

 
 
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.