1743234EN-08

Use of the Main Registers for Simplified Management

Before implementing a motor-starter, it is useful to know which of the main registers are invoked, and in what order.

Diagram of Register Usage

The diagram below provides basic implementation information, using the following registers: configuration, control and monitoring (system state, measurements, faults and warnings, acknowledgment). Starting with the factory configuration (predefined), you will easily be able to follow or anticipate how your system behaves.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?