1743234EN-08

Safety Instructions

CAUTION
HAZARDOUS OPERATION
These devices must be installed, configured and used by qualified staff only.
  • Users must follow all current instructions, standards and regulations.
  • Check the function settings before starting the motor.
  • Do not downgrade or modify these devices.
Failure to follow these instructions can result in injury or equipment damage.
CAUTION
PRECAUTIONS WHEN USING COMMUNICATION VARIABLES
  • Only use the serial link for transmitting data that is not critical to the application.
  • There is some delay in the transmission of data relating to motor-starter states and load-current values. This data must not therefore be used in the management of safety devices and emergency stops.
  • Data such as Forward, Reverse and Stop must not be used in safety and emergency-stop circuits.
Failure to follow these instructions can result in injury or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?