1743234EN-08

General Information on Start-up via the Registers

The LULC033 Modbus communication module settings are implemented or displayed via the Modbus registers.

Access to Parameters

The module I/O parameters are set by using the Modbus RJ45 port, via the application PLC.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?