Warnings - Loss of Communication
Warning Acknowledgment
List of possible warnings.
|
Warnings |
Registers |
LULC033 |
Acknowledgment of a warning |
|
|---|---|---|---|---|
|
460 Warning number |
461 Warning bit |
|||
|
ERR |
||||
|
Thermal overload warning |
4 |
_.3 = 1 |
Off @JLD TBC
|
Automatic when the overload is less than 85% |
|
Loss of communication with the client warning |
109 |
_.15 = 1 |
Flashing |
Acknowledgement by bit 703.3 This bit is active on rising edge and must be reset to 0 by programming. |
Recovery After Loss of Communication
After acknowledgment by setting bit 703.3 to 1, recovery occurs according to the states of control bits 704.0 and 704.1.