Description of the Module and Installation
Diagram of the Module
- 1
-
Green COMM Modbus communication status LED.
- 2
-
Red ERR Modbus communication module fault indication LED.
- 3
-
Green 24V
LED indicating voltage presence
at outputs OA1, OA3, LO1. - 4
-
RJ45 connector for the Modbus RS-485 link.
- 5
-
Connection of the module power supply.
- 6
-
Connection of the 24 V
power supply for outputs
OA1, OA3, LO1. - 7
-
Discrete input 2.
- 8
-
Discrete input 1.
- 9
-
Discrete output 1, assignable depending on the configuration register (685 LSB).
- 10
-
24 V
prewired coil connector
for the power base.-
The assignment of OA1 depends on the configuration register (686 LSB).
-
The assignment of OA3 depends on the configuration register (686 MSB).
-
- 11
-
Connector for communication with the advanced control unit.
Description of Indicator Lights (LEDs)
Description of the various states of the indicator lights (light-emitting diodes, LEDs) on the LULC033 Modbus communication module.
|
Light-emitting diodes (LEDs) |
Meaning |
||
|---|---|---|---|
|
Green COMM LED |
Red ERR LED |
||
|
Flashing (alternately with the ERR LED) |
Flashing (alternately with the COMM LED) |
On |
Bus parameter initialization in progress |
|
Flashing during communication with the Module address |
Off |
On |
Normal operation |
|
Off |
Off |
Off |
Faulty: 24 Vdc voltage missing on the 24 Vdc terminal. Check the connection between the power supply and the communication module. |
|
On |
On |
Internal fault on the LULC033 Internal Faults |
|
|
Flashing |
On |
Loss of communication on the Modbus network |
|
Addressing Using Switches
The Modbus communication module address is defined by switches located on the underside of the module. Turn the module over to access them:
-
The module is delivered with the default address 1
-
Example of configuration with address 20
The range of accepted values is between 1 and 31.
The address coding is in binary format.
The least significant
bit is on the right, indicated by
.
Address 0 is not taken into account by the module, since it is used by the Client for a broadcast request.
Order of Mounting on a Base
The LULC033 module is installed in a power base or a controller base (on the underside of the control unit which locks it in position).
To install the module in the power base or controller base:
|
Step |
Action |
|---|---|
|
1 |
Choose the prewired coil connection terminals. |
|
2 |
Insert the LULC033 Modbus communication module. |
|
3 |
Insert the control unit which locks the module. |