DUG_Exxact MW Push-button Dimmer_WSE-02

Example of an automation

This demonstration shows you how to create an automation to switch on the light with 50% brightness level when a motion is detected.
NOTE: The Dimmer will not be switched off automatically when the Sensor sends the "Unoccupied" message. To switch off the dimmer when there is no more motion, you must create a new automation.
  1. Go to Automation > + to create an automation.
  2. Tap Edit name , enter the name of the automation and tap Save.
    TIP: You can choose the cover image that represents your automation by tapping .
  3. Tap Add Condition > When device status changes > Motion Sensor.
  4. Tap Motion State > Occupied (A).

  5. Tap Add task > Run the device > Push-button Dimmer.
  6. Tap Brightness (B), adjust the brightness to 50% and tap Save.
    TIP: Setting the brightness level turns on the light the light when the automation is triggered. You need not add a task to turn on the Dimmer separately.

  7. Tap Next.
  8. In the Automation Settings page, tap Save.

    Automation is now available under Automation tab. Use toggle switch to enable/disable automation.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?