DUG_Exxact MW Push-button Dimmer_WSE-02

Using the device

The Control Panel allows you to switch the Dimmer On/Off, increase/decrease the brightness and control various settings.

On the Home page, tap All devices > Push-button Dimmer to access the control panel.

On the control panel page, you can see the following:

  • The current state of the Dimmer (A)

  • Sliding bar to adjust the brightness (B)

  • The current brightness percentage (C)

  • Schedule (D)

  • Settings (E)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?