DUG_Exxact MW Push-button Dimmer_WSE-02

For your safety

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Safe electrical installation must be carried out only by skilled professionals. Skilled professionals must prove profound knowledge in the following areas:
- Connecting to installation networks.
- Connecting several electrical devices.
- Laying electric cables.
- Safety standards, local wiring rules and regulations.
Failure to follow these instructions will result in death or serious injury.
DANGER
RISK OF FATAL INJURY FROM ELECTRIC SHOCK
The output may carry electric current even when the load is switched Off.
Disconnect the device from the supply by means of the fuse in the incoming circuit before working on the device.
Failure to follow these instructions will result in death or serious injury.
CAUTION
The device may be damaged
Only connect dimmable load.
Failure to follow these instructions can result in injury or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?