DUG_Exxact MW Push-button Dimmer_WSE-02

Pairing the device with the Wiser Gateway

Using the Wiser app, pair your device with the Gateway/Hub to access and control the device. You can either add the device manually or do an auto-scan to pair it.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?