DUG_Exxact MW Push-button Dimmer_WSE-02

Managing dimmer settings

Using the Wiser app, you can manage the Dimmer modes and settings.

To access dimmer settings:

  1. On the Home page, tap All devices > Push-button Dimmer.

  2. On the device control panel page, tap Settings.

Dimming mode

If you have problems with light flickering, then change the dimming mode in the app. This improves the dimming quality in the light.

Tap Dimming Mode (A) and select either of the following:

Auto - When any other load is connected to the dimmer (e.g. filament bulb).

RL-LED - Select the mode only when the LED is not working properly in Auto mode.

NOTE:
  • Refer to technical data for more information.

  • Flickering may also occur when rotary dimmer is not connected with a neutral wire.

Dimming range

To avoid flickering and switching off the LED, you can restrict the maximum and minimum brightness of the load connected to the device.

Tap Dimming Range (B) and do either or both of the following:

Min Brightness - Drag the slider bar to restrict the minimum brightness.

NOTE: The minimum brightness level should be lower than maximum brightness level.
TIP: If you set the minimum brightness to the right most position on this sliding bar, then the load glows at the minimum brightness even if you drag the sliding bar to the lowest value in the control panel.

Max Brightness - Drag the slider bar to restrict the maximum brightness

NOTE: The maximum brightness level should be greater than minimum brightness level.
TIP: If you set the maximum brightness to the left most position on this sliding bar, then the load glows at the maximum brightness even if you drag the sliding bar to the highest value in the control panel.

NOTE: The Dimming range is limited if the min. and max. levels are too close to each other.

LED indicator mode

You can choose how the LED indicator on the device should work by tapping the LED Indicator mode (C) and select any one of the following:

Reverse With Load - The LED on the Dimmer is On when the device is Off.

Consistent With Load - The LED on the Dimmer is On when the device is On.

Always Off - The LED on the Dimmer is always Off.

Always On - The LED on the Dimmer is always On.

For information on LED color during each modes, refer to LED indication.

Toggle mode setting

Using this setting, the device will remember the last state of the device.

Tap Toggle Mode Setting (D) and select any one of the following:

100% - The LED glows at maximum brightness every time it is turned on.

Last Level (Memory Function) - The LED glows at the previously set brightness level every time it is turned on.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.