DUG_WSE_IPC_Indoor_02

Setting offline notification

Using the wiser app, you can receive a notification when the IP camera is offline.
Follow the steps to turn on the Offline notification:
  1. On the Home page, tap All devices > IP Camera Indoor.
  2. Tap and tap Settings.
  3. Tap the toggle switch (A) to turn On the Offline notification and tap Confirm.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?