DUG_WSE_IPC_Indoor_02

About the device

The Wiser IP Camera Indoor (hereinafter referred to as IP Camera) is a Wi-Fi® operated device that is used to monitor sensitive areas of your home. You can install the IP camera in all directions, e.g. at the ceiling or just put it on a table. The IP camera can be triggered by other Wiser devices.

Advantages of using an IP camera:

  • Increases your overall safety

  • High resolution recording

  • Provides 340° view of the surrounding

  • Infrared night vision for low light recording

NOTE: Users are solely responsible for adhering to applicable privacy laws, e.g. the GDPR, Article 5. Users must ensure that guarantees are taken to avoid any misuse of equipment for surveillance or entirely different and unexpected purposes than intended.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?