Playback
The control panel of the playback consists of:
|
|
Select the recording date and time |
|
|
Click screenshot of the video |
|
|
Pause/play the recording |
|
|
Record the video |
-
A display screen on the control panel shows the previous recordings.
-
The screenshot/recording will be saved in the album.
Recording settings
Follow the steps to change the recording settings:
-
On the Home page, tap All devices > IP Camera Indoor .
-
In the Recording Settings section, tap the toggle switch (A) to enable the Local recording.
NOTE: The recording will be saved to the micro-SD card. -
Tap Recording mode (B) and select one of the options:
NOTE: Recording mode is enabled only when you turn on the Local recording toggle switch.– Event recording - Records only when there is a motion detection
– Non-stop - Records continuously for 24 hours