DUG_WSE_IPC_Indoor_02

Scheduling detection alarm

Using the Wiser app, you can add a schedule that allows you to turn off/on motion detection automatically based on your needs.
Follow the steps to schedule the motion detection:
  1. On the Home page, tap All devices > IP Camera Indoor.
  2. Tap and tap Settings > Motion Detection > Schedule.
  3. Tap Add schedule and set the time (A).
  4. Tap Repeat (B) and select the days you want the schedule to repeat.
  5. Tap Note (C), enter the note and tap Confirm.
  6. Tap the toggle switch (D) to turn On the Notification for the schedule.
  7. Tap Motion detection (E), select one of the options:
    • On - Turns On the motion detection on the scheduled time
    • Off - Turns Off the motion detection on the scheduled time

  8. Tap Save.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?