DUG_WSE_IPC_Indoor_02

Using private mode

The Private Mode allows you to turn off the live view, thereby disabling all the other features on the control panel for all users connected to the same Zigbee network. Using this mode, the user is able to stay confidential during private moments.
Follow the steps to turn On the private mode:
  1. On the Home page, tap All devices > IP Camera Indoor.
  2. Tap > Settings.
  3. Tap the toggle switch (A) to turn On the Private Mode.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?