DUG_Micro Module Shades Control_WSE-02

Creating a moment

A Moment allows you to group multiple actions that are usually done together. Using the Wiser app, you can create moments based on your needs.
To create a moment:
  1. On the Home page, tap .
  2. Go to Moment > + to create a moment.
  3. Tap Edit name (A), enter the name of the moment and tap Save.
    TIP: You can choose the cover image that best represents your moment by tapping .

  4. In the Action section, tap Add task (B) to open the slide-up menu.
  5. In the Add task menu, you can do either or all of the following actions (C):
    • Run the device - Select the devices that you want in a moment
    • Enable or disable on moment creation - Select Automation
    • Delay - Set the delay time
    NOTE: You can add one or more actions using .

  6. Tap Run the device > Micromodule Shutter to select either or all the functions to add in the moment:
    • Control > Shutter Open / Shutter Close (D)
    • Percentage > Set the percentage (E) of moment required.

  7. Once all the actions are set, tap Save.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?